This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR65NEVM: NIR DMD

Part Number: DLPLCR65NEVM
Other Parts Discussed in Thread: DLPLCRC410EVM, DLPC410

I am planning to build a complete NIR DMD system.

What are the components should I buy ?( except the lens, light source and power supply, we have these components)

On hand I have found parts:

1. DLPLCR65NEVM

2. DLPLCRC410EVM

  • Hello Eddy,

    From a hardware standpoint that is what you will need to start with.  You will want to download the test software GUI so you can test that the mirrors are working.

    Depending on the optical power you plan to use you will need to determine the thermal solution needed to cool the DMD.  It comes with a small thermal plug with two threaded holes to mount a larger heatsink.

    From a software point of view, is you wish to run at high speeds, you will need to employ a good FPGA programmer.  The controller EVM does have a memory slot.

    The EVMs are for evaluation.  If you decide to design a product, you may want to consider a newer front end FPGA to drive the DLPC410.

    Please send a friend request if you would like to discuss more private details about a product you would like to build.

    Fizix