Other Parts Discussed in Thread: DLP3010EVM-LC
Hello,
We are trying to project a pattern (Solid color) with DLPC3478 with specific amount of time. Exposure time minimum 10 ms maximum 100 ms. Also we want to set trigger output without loading internal pattern because we use interal patterns for something else. Also we want to project pattern only once after command has been sent. Because if connection with dlpc lost, pattern projection should stop. What can we do?
Best regards,
Bayram