Other Parts Discussed in Thread: DLPC6540, DLPC4422
Hi E2E team,
we want to run DLP471TPEVM at 1920x1080@240 Hz, which should be supported by DLPC6540/DLP417TP.
EVM itself runs fine, including GUI v.3.2.0.6.
We feed HDMI2.0 signal from a NVIDIA Quadro RTX4000 and see 2160p@60 as well as 1920x1080@60.
EDID does not contain a 1920x1080@240Hz mode, when feeding a custom 240 Hz mode such as
PixelClock=599.574 MHz, HActive 1920, HSyncStart 2112, HSyncEnd, 2204, HTotal, 2292, VActive 1080, VSyncStart 1085, VSyncEnd 1086 VTotal 1090
D1 on the Formatter board goes on (V-by-One LOCK = TRUE), but no image is displayed.
I assume that we need a mode which is accepted by the DLPC6540 and probably an EDID which contains this mode. How should we proceed?
Thank you,
Matt