This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: Customised PCB

Part Number: DLP3010EVM-LC
Other Parts Discussed in Thread: DLPA2005, DLPC3478, DLPC3479

We are designing a custom PCB for our project. The idea is to customize the display board and main board PCB into a single PCB within certain dimensions (user requirement), to produce an array of 1D patterns at a fixed rate and also trigger cameras. Consider we have purchased DLPC3478, DLPA2005, MSP430, Cypress IC and Flash IC individually.

Using the GUI, we would set a pattern and its order, other configuration details along with trigger information and then select the ‘Program and Load Pattern’. Post this we take a backup of the firmware. Considering the above scenario kindly answer the below queries-

  1. The downloaded firmware image is to be programmed to which IC – Flash Memory or DLPC3478?
  2. Is there any coding required for DLPC3478/ DLPA2005?
  3. How do we program MSP430 to send PROJ_ON signal to DLPC3478?

Also kindly let us know if anything is missed out for making the customised PCB functional.