Hi,
I am trying to configure my DLP4500 with the LightCrafter 4500 Control Software. I set up my pattern sequence, saved it as a solution, and created a new firmware with this solution so that I don't have to set my sequence again. I uploaded this firmware on the projector and now it automatically enters pattern mode and is projecting the pattern. The problem is that the LightCrafter 4500 Control Software can no longer detect the projector.
I have tried:
1) Resetting the projector (pressing the reset button on the board)
2) Restarting the projector (plugging it on and off again)
3) Putting the projector in Standby mode and back
4) Unplugging and replugging my USB connection
5) Closing the Control Software and opening it again.
Nothing has worked so far.
Here's my .ini file for reference:
APPCONFIG.VERSION.SUBMINOR 0x0 ; APPCONFIG.VERSION.MINOR 0x0 ; APPCONFIG.VERSION.MAJOR 0x3 ; DEFAULT.FIRMWARE_TAG 0x0 ; DEFAULT.AUTOSTART 0x0 ; DEFAULT.DISPMODE 0x1 ; DEFAULT.SHORT_FLIP 0x0 ; DEFAULT.LONG_FLIP 0x0 ; DEFAULT.TRIG_OUT_1.POL 0x0 ; DEFAULT.TRIG_OUT_1.RDELAY 0xbb ; DEFAULT.TRIG_OUT_1.FDELAY 0xbb ; DEFAULT.TRIG_OUT_2.POL 0x0 ; DEFAULT.TRIG_OUT_2.WIDTH 0xbb ; DEFAULT.TRIG_IN_1.DELAY 0x1 ; DEFAULT.TRIG_IN_2.POL 0x0 ; DEFAULT.RED_STROBE.RDELAY 0xbb ; DEFAULT.RED_STROBE.FDELAY 0xbb ; DEFAULT.GRN_STROBE.RDELAY 0xbb ; DEFAULT.GRN_STROBE.FDELAY 0xbb ; DEFAULT.BLU_STROBE.RDELAY 0xbb ; DEFAULT.BLU_STROBE.FDELAY 0xbb ; DEFAULT.INVERTDATA 0x0 ; DEFAULT.TESTPATTERN 0x1 ; DEFAULT.LEDCURRENT_RED 0x97 ; DEFAULT.LEDCURRENT_GRN 0x78 ; DEFAULT.LEDCURRENT_BLU 0x7d ; DEFAULT.PATTERNCONFIG.PAT_EXPOSURE 0x208d ; DEFAULT.PATTERNCONFIG.PAT_PERIOD 0x208d ; DEFAULT.PATTERNCONFIG.PAT_MODE 0x3 ; DEFAULT.PATTERNCONFIG.TRIG_MODE 0x1 ; DEFAULT.PATTERNCONFIG.PAT_REPEAT 0x1 ; DEFAULT.PATTERNCONFIG.NUM_SPLASH 0x15 ; DEFAULT.SPLASHLUT 0x0 0x1 0x2 0x3 0x4 0x5 0x6 0x7 0x8 0x9 0xa 0xb 0xc 0xd 0xe 0xf 0x10 0x11 0x12 0x13 0x14 0x15 ; DEFAULT.PATTERNCONFIG.NUM_LUT_ENTRIES 0x41 ; DEFAULT.PATTERNCONFIG.NUM_PATTERNS 0x41 ; DEFAULT.SEQPATLUT 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 0x62808 0x22800 0x22804 ; DEFAULT.LED_ENABLE_MAN_MODE 0x0 ; DEFAULT.MAN_ENABLE_RED_LED 0x0 ; DEFAULT.MAN_ENABLE_GRN_LED 0x0 ; DEFAULT.MAN_ENABLE_BLU_LED 0x0 ; DEFAULT.PORTCONFIG.PORT 0x0 ; DEFAULT.PORTCONFIG.BPP 0x1 ; DEFAULT.PORTCONFIG.PIX_FMT 0x0 ; DEFAULT.PORTCONFIG.PORT_CLK 0x0 ; DEFAULT.PORTCONFIG.ABC_MUX 0x4 ; DEFAULT.PORTCONFIG.PIX_MODE 0x1 ; DEFAULT.PORTCONFIG.SWAP_POL 0x1 ; DEFAULT.PORTCONFIG.FLD_SEL 0x0 ; PERIPHERALS.I2CADDRESS[0] 0x34 ; PERIPHERALS.I2CADDRESS[1] 0x3a ; PERIPHERALS.I2CBUSYGPIO_ENABLE 0x0 ; PERIPHERALS.I2CBUSYGPIO_SELECT 0x0 ; DATAPATH.SPLASHSTARTUPTIMEOUT 0x1388 ; DATAPATH.SPLASHATSTARTUPENABLE 0x0 ; MACHINE_DATA.COLORPROFILE_0_BRILLIANTCOLORLOOK 0x0 ;
In case you want to try running it yourself to see if you can replicate the issue, you can find the firmware here: drive.google.com/.../1NReK4L5ij6NxpKnonPOWuN65_7C_ofqG
The only thing I think I might have done to break it is to automatically enter pattern mode. What could be the issue and how do I solve it?