This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3479: About Exposure Time Range

Part Number: DLPC3479
Other Parts Discussed in Thread: DLPC3478

Dear Mayank-san,

The exposure time range of the DLPC3479 is 1677 to 4168 in 8-bit monochrome in internal pattern mode, but does it not support a wider range (such as 29012us) like the DLPC3478?
Or are there any plans to support it?

Best Regards,
Kadowaki