This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP NIRscan Nano EVM - Scan issues

Hello, I am an end user of the DLP Nano EVM device and I cannot find any information about the problem that could help me resolve it.

The image below shows a reference sample signal in Wavelength and Index. After the index of the second measurement (Wavelength 906.02nm) and at each certain Wavelength measurements (24) the intensity is not detected and the results are expressed in insignificant values. This problem occurs at 10 different points across the spectral range (900 to 1700nm).

Index Interval (index) Wavelength (nm)
2 - 906,0
26 24 1000,9
50 24 1094,3
74 24 1185,1
98 24 1272,0
122 24 1357,3
146 24 1440,0
170 24 1519,9
194 24 1596,1
218 24 1670,6

How to fix it? Can anyone from the community help me resolve this issue?

Regards,
Daniel