This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM: Humidity Protection

Part Number: DLPLCR4500EVM

Hello,

I would like to set up an experiment with my DLP Lightcrafter 4500 in an incubator, but I am concerned that the humidity would damage the exposed electronics.  I am considering designing a water-tight casing for the Lightcrafter that the lens of the lightcrafter would stick through.  This means that the lens would be exposed to the humidity in the incubator. Is this part of the Lightcrafter water tight or would the entire device need to be boxed in from the humidity?

Best,
Michael