Other Parts Discussed in Thread: DLP4710LC
Hi,
I'm using a DLP projector from Wintech named PRO4710LC-405-92. It uses the DLP4710EVM-LC, and at first I managed to project a purplish light via the DLP LightCrafter Display v7.4 - 4710EVM GUI (I always seem to get the following error message too):
At that point I could run the splash pattern and even display external video, but as I attempted to project other colors (I only ever managed to display the purplish light), the projector stopped displaying any kind of output altogether.
As far as I know, the only thing I ever changed was the firmware version, I've tried with 7.0.1, 8.0, 8.1.0 and 8.0.1, but no matter what I do I can't get the projector to display anything.
While powering the projector the following pins light up, including the pin D36 which I've searched and apparently indicates that the projector is connected to the PCB:
I also switched to DLP EVM GUI 3.2.0.6 as I seem to get more data in this interface:
I don't know if there is something wrong with the projector itself, if it's the firmware version that causes the issue, or if there's something else I've been doing wrong, but I would thank any suggestion that might shed some light on the matter.