Other Parts Discussed in Thread: DLPC900, DLPC910, DLPC4430, DLPC4422, DLP650NE, 4430
Hello,
Currently, I prepare to lauch a project of DMD. Here are some question I want to know.
1, Can I use DLPC4420 to replace DLPC900 to drive dlp6500? If yes, Could you recomend some reference design?
2. Can DLPC4420 configure HDMI bridge chips through its built-in I2C?Include work mode and EDID information which is in HDMI bridge chip.
3. DLPC4420 comes with its own program, so we don't need to develop software, do we?
4. If dlpc4420 can drive dlp6500, can it be used 0.65_ 1080p_ GUI by usb interface?
Perhaps there are some unreasonable question, please forgive me a lot.
Thanks!
Sunny