Hello, TI engineer !
We use Internal Pattern Streaming mode, and constantly use I2C to trigger instructions (the instruction is run once), and the interval between instructions is 100ms. After giving the trigger instruction for a long time, the display of internal patterns will stop after a few hours, and the time is random. At this time, only restart the power supply to restore the solution.
Is this a known Bug and how can we solve it?
Because I noticed that in Pico Firmware Selector, 3478 version 9.0.1 firmware has been released, which mentioned that similar problems have been solved.
Thank!