Hi,
・I removed a DMD board from LightCommander.
・The board was returned, and it was operated again.
However, LED did not light.
・Check the connection of the DMD board was found that floating a little bit from the socket
・LED lit when the board was correctly inserted into the socket.
I would like to ask a question.
1. Is it a normal control of DLPC200 that LED doesn't light for the communication trouble to DMD (loose connection)?
2. Is there a reason why some LED is not lit?
Regards,
Seishin