I am planning to use the DLP7410 in a spectrometer. I know that the working spectral range is ~400 to 700 nm, but what limits the longer wavelength.
Is it the AR coating on the cover glass or is it related to the Mirrors themselves.
Also, I know that there is a development module DLPDLCR4710EVM-62, but this is more elaborate than I need. Is there a simpler platform with just the DLP and driver chips?