This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC230-Q1: Vcm problem for IBIS model

Part Number: DLPC230-Q1
Other Parts Discussed in Thread: SN65DSI83

Hi,

I am using LVDS input pin model (fxlvrx020hh0l-odt1-rx-p and fxlvrx020hh0l-odt1-rx-n) of DLPC230-Q1, and found Vcm is ~3.3V when 0~1V differential voltage, this exceed datasheet Vcm requirement (min 0.35V, nom 1.2V, max 1.6V), so how to solve this model problem? thanks

the circuit and Vcm waveform as below figures.