This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: I2C input hysteresis?

Part Number: DLPC3478
Other Parts Discussed in Thread: DLPC350

The data sheet states that the input of the I2C (e.g., IIC0_SCL) of the DLPC3478 is hysteresis.
However, its level is not prescribed.

The DLPC350 data sheet states VHYS(VT+ - VT-)=550mV.

What are the specifications of the DLPC3478?