There are Table 3-82 and Table 3-83 in "3.4.9 Write Pattern Order Table Entry (98h)" of "DLPC3479 Software Programmer's Guide (Rev.B)", which one is correct?
Or is Table 17 of Rev.A correct?
Best Regards,
Kadowaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are Table 3-82 and Table 3-83 in "3.4.9 Write Pattern Order Table Entry (98h)" of "DLPC3479 Software Programmer's Guide (Rev.B)", which one is correct?
Or is Table 17 of Rev.A correct?
Best Regards,
Kadowaki
Hello Kadowaki,
Thank you for pointing this extra table out, I will make note and make sure this gets updated. The DLPC3479 does not currently support 4-bit, 5-bit,6-bit internal patterns. The correct table is as follows:
Bit depth | Vertical | Horizontal |
1-bit |
64 | 60 |
8-bit | 8 | 7 |
Best,
Maximus
Dear Maximus-san,
Thank you for the reply.
The reply email said to use "DLPC3479 Software Programmer's Guide (Rev.A)", but Table 17 shows 60 patterns (1 bit) and 7 patterns (8 bits) for "horizontal" .
Which is correct, the table above or Table 17 of Rev.A?
Best Regards,
Kadowaki
Hi Kadowaki,
You are correct, it should be 60 (1bit) and 7 (8bit), I will correct my chart above.
Best,
Maximus