Other Parts Discussed in Thread: DLP4710LC, DLP4710, , DLPA3000, DLPC3439
Hello, TI experts:
My system is designed with reference to dlpc4710lc, using also dlpc3479+dlpa3000+dlp4710lc, I send the corresponding IIC commands with reference to the GUI instruction manual that comes with the evaluation version and the programming guide of the dlpc3479 software, but the dlp4710 can't be displayed in accordance with the IIC commands that I send it to, which gives me the following problems that
Question 1: What kind of IIC commands do I need to send from my side to get the system to perform the simplest internal pattern display;
Question 2: Does the WriteGPIO[19:00]Control (0x31) command on this side control the gpio port output of the dlpc?
Question 3: Can I control the voltage output of Vled by sending Write RGB LED Enable (0x52) instruction from my side?
Thanks
Alexander