Hello.
I am using a DLP7000. It has a usable wavelength of 400-700nm and a micromirror pitch of 13.68㎛.
The light source is a multimode laser diode with a wavelength of 450nm.
Currently, I have tried to set up the projection optics with a single biconvex spherical lens, but it does not handle diffracted light well.
When using a DMD with a coherent light source, diffraction will occur, so how should the optics be designed to collect only the zero-order or up to ±1st- order light?
Thank you in advance.