This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP6500FLQ:DLP S600

Part Number: DLP6500FLQ
Other Parts Discussed in Thread: DLPC900

在使用GUI界面控制DMD时,选择模式时都会报错,unable to switch ...模式。之前将USB连接电脑之后,闪退过一次,再次打开,就会出现这种情况。请问怎么解决呢,是什么造成这种情况呢?

  • Dear ? ??,

    Similar to Fizix's response in another thread you have posted recently, you may want to post in the China E2E forums, as that may be more productive for you.

    Here is what Texas Instruments' translation tool has translated for me:

    "When using the GUI interface to control the DMD, an error is reported when the mode is selected, unable to switch... mode. This occurs when the USB is connected to the computer and then turned back on again after flashing it once. How can we solve this situation and what is causing this situation?"

    Is this a correct translation?

    Regards,
    Michael Ly

  • yes,it is a correcttranslation.So,I should how solve this situation,thank you.

  • Hello ? ??,

    Am I also correct in assuming this is a custom board design for the DLP6500FLQ? I see the image on your GUI uses a mustang flex cable instead of the HPC FMC cable we use on our DLP6500FLQEVM.

    It looks like you have edited the source code provided with our GUI to create DLP VisionFly 0.65 1080p 2.0.0? Have you attempted to use our latest GUI and firmware for the DLPC900 on this? Here is a link to the reference software. Please let me know if this latest version recognizes your DMD.

    Let me check with our firmware expert if the DLPC900 firmware will recognize the DLP6500FLQ as well.

    P.S. If you did modify our GUI, what version of our GUI did you modify? That may help us if we are unable to find a solution sooner.

    Regards,
    Michael Ly

  • Hello, DMD uses.65 "1080p 2xLVDS S600 DMD(I don't know the specific model, the data manual is given by the teacher, as follows. If TI experts know, it is convenient to inform), the controller is DDP4422, the controller data manual I did not find on the official website. The flexible cable is shown below. Not using the latest firmware and GUI. Below is a diagram of the controller and DMD used.

  • Hi ? ??,

    I'm sorry, but Texas Instruments cannot support you with this, as you are using both custom hardware and software. This is not a TI DLP(R) product. You will have  to contact the party that developed the VisionFly GUI you are using and the person or party who designed the DDP4422 board you are using.

    The DMD you are showing is a DLP6500NEFYE, and not a DLP6500FLQ. This is a display part that is supported by a display controller such as DDP4422 or DDP4422-HV.

    The DLPC900 does not support this DMD shown. The display controllers (such as the DDP4422) do not run DLPC900 firmware, thus they will not work with the DLPC900 GUI.

    On top of  that, the DDP4422 controller does not support Advanced Light Control (ALC) functions that the DLPC900 offers. This means you are not able to use triggers, control exposure time, etc... If you wish to have those functions with the DLPC900, you would need to purchase a compatible chipset.

    Regards,
    Michael Ly

  • Hi again ? ??,

    I am marking this thread as resolved because the solution here is to talk with the developer of your custom DDP4422 board and the modified GUI. TI cannot provide further support because we did not design the board shown and do not know what edits have been made to the GUI in question.

    If you have any other questions,  you may open  this thread back up within 14 days.

    Regards,
    Michael Ly