Hello I just entered in the community but work already since a year with the d4100.
In the Extranet that I have access to, I see:
"DDC4100 Application FPGA Sample Code"
"DDC4100 Application FPGA Sample Code for GUI use"
These two zips contains numerous files but none of these files seem to contain any C code or an obvious DLL I can use to control the D4100 through an external program.
Is there an header file somewhere to start development over d4100explorer This would be extremely helpful.