This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: Internal Pattern Streaming image projection order is wrong.

Part Number: DLP3010EVM-LC

Hi,

I am encountering a phenomenon where images are not projected in the correct order when Internal Pattern is set in the DLP EVM GUI.

Even if the graycode pattern is set in the order of fineness, it will be projected in a different order when start with the "Run Once" command.

I have tried rewriting the firmware, reinstalling the EVM GUI, and reconfiguring the pattern. These have no impact.

How do I solve this?

EVM Software : 9.0.0
Firmware : 9.0.1
GUI Software : 3.2.0.6.

  • Hello Kenjiro,

    This is due to a bug we have found with the "Pattern Set Entry Index" added in this firmware release. We are working on a maintenance release to address this issue. In the meantime instead of this index being = 0 in your pattern sets please increase it to = 1. This should give you the default order you are expecting.

    Best,

    Maximus

  • Hello Maximus,

    Thank you for your reply.

    I confirmed that the problem was resolved by changing "Pattern Set Entry Index" to 1.

    Best regards,
    Kenjiro