Other Parts Discussed in Thread: DLPLCRC900DEVM, DLPC900
Hello Team, one of our customer bought DLPLCR90EVM and DLPLCRC900DEVM from us and claims they are not working properly. Before they confirm these parts are defective they want to troubleshoot. Their explanation is following,
-----------------
I ordered two things, one is DMD DLPLCR90EVM and another is evaluation board DLPLCRC900DEVM. Both are connected using flex cables but when I do, according the user guide, the DMD should light up. it does not happen. However I saw that the evaluation board D5, D11 D12 light up, D7 toggles but D9 does not. Which I missed the last time to notice. I am attaching a video and a picture of the evaluation board, dmd however even if I connect does not light up. I am scared to connect them, as I feel it might damage the evm.
-----------------
Can you please advise how can we troubleshoot this issue?