Other Parts Discussed in Thread: DLP3020-Q1, DLPC120-Q1, DLP3021LEQ1EVM
Hello,
The two 0.3 inch automotive DLPs DLP3021-Q1 and DLP3020-Q1 have very similar specifications with both sharing the same package and resolution.
While one product is recommended for interior display and the other for exterior display, what is the actual technical difference between these DLP-s?
I see that the recommended controllers differ -- DLPC120-Q1 is referenced with DLP3020-Q1 and an FPGA with DLP3021-Q1.
Does it mean that these controllers are incompatible between these DLP models?
Thanks,
Andreas