Other Parts Discussed in Thread: DLP4710, , DLPC3479
Hello,
I have a few questions regarding connecting a microcontroller to DLP4710 and trying to communicate over I2C.
- From the schematics it looks like that I need to short/put 0 ohm resistors on R177 and R178 to connect to J11 for I2C communication. Is this correct?
- Do I need to change the functionality of SW21 by pressing and holding it?
- If the I2C channel is a multimaster bus with the Cypress and MSP430 as the masters, do I need to connect a microcontroller that supports multimaster or just a normal microcontroller such as an arduino would be fine? How does this would work? Would MSP430 still function as a master? Could you please elaborate?
Thank you for the help.