This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP7000UV: Spec of Cover glass

Part Number: DLP7000UV


Hello
I am designing a laser processing machine using DLP7000UV.
We are currently in the process of creating and experimenting with a prototype.

I would like to accurately calculate the distance between the DMD mirror and the imaging lens.
What is the thickness of the cover glass of DLP7000UV?
What is the material and refractive index of the glass?

Thank you for your advice.

  • Hello Taka,

    This information can be found in the data sheets and its attached ICD.

    The cover glass per the data sheet [DLPS061E] in  7.13 Window Characteristics on page 21 is Corning 7056.  You will have  to get the specifications from Corning for this glass.

    For distances see the ICD attached to the data sheet.  Sheet 1 shows the thickness as 2.9972 +/- 0.127 mm.  The gap between the active array surface is right there also shown as 0.48626 +/- 0.1524 mm.

    Fizix

  • Hello Fizix,

    Reply Thank you very much.
    This information will be very helpful.
    I will proceed with the design based on this information source.

    Nice to meet you again.