This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP651NE: dithering and flickering question

Part Number: DLP651NE
Other Parts Discussed in Thread: DLP9500, DLPC7540, DLPC410

Hello

Please kindly provide a response for my listed questions on DLP651NE:

1- what is the flat state angle on DLP651NE (-12 degree?!)

2- does DMD dithers in Off and Flat sate as well.

3- what is dithering range in angle in On-State, Off-Sate , and Flat state? 

4- what is the dithering speed (frequency) in On-State, Off-Sate , and Flat state.

Background info: 

We have a camera in system that at low exposure time,  it starts to capture DMD dithering in  off-state. We can see beating frequency between two system: By knowing above question we can do a better job in blocking scattered light in off state and change exposure frequency to get rid of beating frequency....

This is kindly urgent. Appreciate for quick response. Please point me to data sheet or any other document if I missed it. 

Thank you

Babak

 

  • Babak,

    The Flat state is not used during normal operation; it is only used when the system is powered down (or the DMD is "parked").  

    On/Off is nominally +/- 12 degrees (normal to center of the DMD array, diagonally/corner-to-corner; +/- 1 degree tolerance).  ON is nominally 24 degrees away from OFF.

    Section 6.11 in the datasheet describes the mirror performance.  The crossover time (between ON and OFF) is nominally 2.5us; the minimum switching time is 8us:

    The actual time between mirror transitions will generally vary between ~8us and ~400us.

    Was there some other information you were looking for?

    Regards,
    Gary

  • thanks for your response... it answered partially my questions. I need to know on dithering.

    1-A- you said "he actual time between mirror transitions will generally vary between ~8us and ~400us." why 400us. you mean to scan through entire mirrors or each mirror takes 8-400um. 

    1-B ==> mirror transition in series or in parallel- all at once-? 

    2- does DMD dithers in Off and Flat sate as well.

    3- what is dithering range in angle in On-State and Off-Sate ? 

    4- what is the dithering speed (frequency) in On-State, Off-Sate.==> is it like 2.5us too?

    thanks

    Babak

  • Babek, 

    > 1-A- you said "The actual time between mirror transitions will generally vary between ~8us and ~400us." why 400us. you mean to scan through entire mirrors or each mirror takes 8-400us. 

    This is the time between bit patterns.

    >    1-B ==> mirror transition in series or in parallel- all at once-? 

    This document describes the general concepts of how the DMD operates.  It describes several modes (Single, Double, Quad, & Global); we only use Global  Mode and Single Block Mode with Phased Operation (sequentially, from top to bottom) on this product.

    DMD 101: Introduction to Digital Micromirror Device (DMD) Technology (Rev. B)

    The mirrors can all change state at roughly the same time ("global"); or they can change state in groups ("block", "group", or "phased").  This DMD has 12 groups/blocks of 90 rows each (12 x 90 = 1080).  (Note: Different DMDs have different numbers of groups/blocks.) 

    In the case of a phased bit/reset, the entire DMD is updated from top to bottom 90 rows at a time sequentially (12 groups).  The individual groups are typically skewed ~3.0 - 4.5us.  The skew from top to bottom is typically ~40-50us.  

    In the case of a global bit/reset, all of the mirrors move at roughly the same time (there is actually a small internal skew; ~1us from top to bottom).

    The majority of the bits are phased; global resets are typically only used for color transitions.

    > 2- does DMD dithers in Off and Flat sate as well.

    The DMD is a bi-stable device; it only operates in the ON and OFF states.  The flat state is only used for power-off/park.

    > 3- what is dithering range in angle in On-State and Off-Sate ? 

    On and Off are nominally 24 degrees apart from each other (or nominally +/- 12 degrees from normal). 

    > 4- what is the dithering speed (frequency) in On-State, Off-Sate.==> is it like 2.5us too?

    The transition time between ON and OFF (the time while a mirror is moving) is nominally 2.5us.

    The time for the DMD to update from top to bottom is typically between ~1us (global) and ~40-50us (phased).

    The time between bit patterns is typically between ~8us and ~400us.

    I believe all of the times I have mentioned should reflect the general case with the flash images provided for the EVMs; although I have not looked at every possible case.


    Regards,
    Gary

  • well explained ....thank you... now I understand my problem. Last question  on what we see in our test:

    Question 5-
    - DMD dithers to avoid sticking of mirrors. correct? 
    - And now if DMD is in ON State and since DMD only have two state: What is the duty cycle  of dithering in ON state?  like 99% ON (mirror stay in +24 degree) and 1% Off (-24 degree). and what is the full period of dithering in msec or usec

    Samwise, What is the duty cycle  of dithering in OFF state?  like 99% OFF (-24 degree) and 1% ON (+24 degree).

    asking as we dump the beam  to empty space so no scattering coming to system but we see some beam comes back to system in dithering frequency... it has a beating pulse.. 
    Please let me know what is the Ona nd Off duty cycle for dithering. And can we change the duty cycle. we need to have minimum duty cycle in ON mode  when we are OFF state to have almost zero background.


    we want to know this % and if we can change it... 
    thanks for response

    I am waiting thanks 

      

  • Ahh, I see where some confusion is.  What we call "dithering" is a part of the process of converting the video input to PWM patterns that we can display on a DMD.  What you are referring to is not a part of what we call "dithering"; the pulses you are referring to are inserted for other reasons that are not display related.  These pulses are not displayed as the illumination is off during these pulses (all of the illumination enables should be off during this time).

    There is a pair of mirror transitions inserted once per frame at the start of the first blue segment; they are about 1% of the frame time.  The time is split roughly in half for ON and OFF (i.e. roughly 0.5% ON and 0.5% OFF).  The on time should always be ~0.5%; the off time should be the greater of 0.5% or ~60us for this particular dmd and controller.  You cannot change the duty cycle of these pulses.  

     

    Also... I noticed that you mentioned -24 degree and +24degree...  the DMD moves +/-12 degrees (nominally), NOT +/- 24 degrees.  The total movement is 24 degrees (nominally) between on and off.

    Regards,
    Gary

  • Hi Gary I am totally confused... 
    Ok +/-12 degree... no problem....
    I can not understand this

    There is a pair of mirror transitions inserted once per frame at the start of the first blue segment; they are about 1% of the frame time.  The time is split roughly in half for ON and OFF (i.e. roughly 0.5% ON and 0.5% OFF).  The on time should always be ~0.5%; the off time should be the greater of 0.5% or ~60us for this particular dmd and controller.  You cannot change the duty cycle of these pulses.  

    I want to know does mirror in either ON state or OFF state, has to constantly move to avoid sticking ==> I hear something like this or it is not true

    I also want to know if mirrors are at off state do they move/vibrate/go back and forth to some extend or not. if they do I want to know  what is the duty cycle of it. according to earlier discussion mirrors are either at +12 degree or 0 (flat) or -12 degree and we do not have anything in between. we are observing some frequency modulation when we put DMD at -12 degree to be off. but it seems it is vibration (we call it "dithering"... you tell me what to call it). 
    thanks

    Babak
    do you want to call me than back and froth and more confusion. i give you my cellphone. thanks 

  • Banak,

    No, the mirrors do not have to constantly move.  We do force them to move one time per frame via the pulses I described above. 

    If you input all black video data, the mirrors will remain in the off state for -99.5% of the frame; they will move to the on state for ~0.5% of the frame time once per frame (the pulses I described above).  

    If you input all white video data, the mirrors will remain in the on state for ~99.5% of the frame time***; they will move to the off state for ~ 0.5% of the frame time (again, these are the pulses I described above).  As I detailed above, this will actually be the greater of 0.5% or ~60us.

    All three illuminator enables should be low when this occurs; so you could use them to identify and measure the behavior using a photo detector or high speed camera, etc..

    ***This is a video system with gamma, dithering, color processing, etc.; so even with full white, some pixels may be off for short times due to the various algorithms.  (There is a recent e2e question about that, I think.) 


    Also keep in mind that there is a pwm sequence always running, loading data and generating mirror clocking pulses even if the input data is unchanged.  Every ~8us to ~400us, data is loaded and mirror clocking pulses generated.  This may cause the mirrors to wiggle or deflect slightly from their on or off positions.  This has no impact on video display systems; but it can be measured and it can affect non-display applications that have very high f/# (f/10, f/20 or more; display systems typically operate at less than f/3).  

    Regards,

    Gary

  • Ok now we are talking....
    so I graphically plotted above what % in constant On/Off state mirrors flip or swing or what I called it "dither".

    please confirm or reject my logic below. This is what I understand form you==>

    A- Although mirrors stay 99.5% On/Off states, a pwm sequence always running, loading data and generating mirror clocking pulses. As a result, even if the input data is unchanged,  like I am always On or always Off,   This may cause the mirrors to wiggle or deflect slightly from their on or off positions. like 99.5% On/Off and 0.5% Off/On. 
    B- this pulses are approximately generated every ~8us to ~400us, data is loaded and mirror clocking pulses generated

    is above what I said correct? thanks for Ye or Ne

    is this any different that DLP9500. I am comparing our cheap  DLP651NE to ur more expensive version DLP9500.... thanks 

    Babak

  • Babek,

    > is above what I said correct? thanks for Ye or Ne

    Yes and no...

    > A- Although mirrors stay 99.5% On/Off states, a pwm sequence always running, loading data and generating mirror clocking pulses.

    Yes, the memory DMD is always loaded and resets (clocking pulses) generated.

    > As a result, even if the input data is unchanged,  like I am always On or always Off,   This may cause the mirrors to wiggle or deflect slightly from their on or off positions. like 99.5% On/Off and 0.5% Off/On. 

    No, not exactly....this is not like the 99.5% on/off case.  The mirrors do not move to to the opposite state.  My understanding is that they move roughly half way to the flat state (~4-6 degrees) and return within 1-2us or less.  This does not affect the vast majority of applications; in a display or most structured light applications, it is not an issue.  In very high f/# applications, it can be a problem.

    > B- this pulses are approximately generated every ~8us to ~400us, data is loaded and mirror clocking pulses generated

    Yes, the PWM sequence will load and reset (generate "mirror clocking pulses") every ~8us to ~400us, independent of what the input data is and what is already displayed.

    is this any different that DLP9500. I am comparing our cheap  DLP651NE to ur more expensive version DLP9500.... thanks 

    Yes, it is quite different.

    The DLP651NE uses the DLPC7540 controller.  The 7540 is designed for video display applications; it does not give you control over individual patterns displayed on the DMD.  It runs in a mode that is designed to continuously display live video data.  

    The  DLP9500 works with the DLPC410 controller.  The DLPC410 is designed for applications that need specific control of the individual bit-patterns displayed.  It does not have any video processing.  It does not run a PWM sequence.  It takes a single bit pattern and displays it when you tell it to.  The EVM includes an apps FPGA that allows some basic loading of patterns through USB through a scripting interface.  The source for the Apps FPGA is provided in the event someone wants to modify it to take an external input, add external memory, etc..  There are also various modules and kits available from different partners, some with more advanced features (storage of multiple patterns, etc) available:  https://www.ti.com/product/DLP9500?gclsrc=aw.ds#design-development 

    Regards,
    Gary

  • thanks Gary... we are almost done......

    in short  I am comparing DLP9500 vs DLP651NE... do we see any 99.5% on/off and 0.5% flat/flat (~4~6) case when we are holding DMD in On/Off state? 

    we are purchasing currently both DLP9500 and DLP651NE

    thanks

    Babak

  • Babel,

    With the DLP9500 and the DLPC410 controller, the mirrors only move or attempt to move when you tell them to.  If you leave them set to off, they will stay off.  Note:  I believe there are some data-sheet rules or recommendations around how long you should leave them on or off.

    Keep mind that if you are displaying a pattern and then you load the same pattern and generate a mirror clicking pulse (reset), or you just command a reset, the mirrors will move roughly half way to flat and back over ~1-2 us.  

    Regards,

    Gary

  • aha... so DLP9500 differs from DLP651NE that the mirrors only move or attempt to move when you tell DMD to do so when Data is loaded, when we want it to (of course following some data-sheet rules or recommendations around how long you should leave them on or off). While in LP651NE  every ~8us to ~400us, data is loaded and mirror clocking pulses generated which causes DLP651NE move roughly half way to flat state. This does not occurs for DLP9500 when mirror are kept at On or Off stated as there is no  PWM sequence. (again this is of course following some data-sheet rules or recommendations around how long you should leave them on or off) . It is as in case of DLP651NE due to nature of Video control board , a PWM is always running in DLP651NE as loading data and generating mirror clocking pulses  every ~8us to ~400us. 

    if above is correct I close the case. I need your confirmation to get my narrative correct to report to VP of engineering. 
    thanks

    if above is true... mirror function in DLP9500 doe snot need to move (of course following some data-sheet rules or recommendations around how long you should leave them on or off). I heard in all DMD mirrors have to move back and forth constantly (On/Off mode to flat state) else mirror stick and will not function... perhaps info was not correct. Now you know why I repeat my question and need your/expert confirmation. than following chats on internet or verbal/tribal knowledge. I need engineering facts. 

    thank you

    Babak

  • Babak,

    The difference is the intended use and markets for the products.  

    The DLP9500 works with the DLPC410 controller.  This solution is for "Advanced Light Control" (ALC) applications where control of the individual binary patterns displayed is required.  That specific controller only supports loading the DMD and triggering rests (mirror clocking pulses) when commanded by the front-end/user.  It does not understand live video, color, gamma, etc.. 

    The DLP651NE works with the DLPC7540 controller. This solution is specifically for video display.  The DLPC7540 is specifically designed for video display applications where full color / gray-scales need to be displayed.  It has various algorithms for that purpose (gamma, color processing, dithering, etc.).  It runs in a continuous mode, expecting a continuous Vsync and live video data.  It runs a pwm sequence that is designed for continuous display of video data and typically has loads and resets (mirror clocking pulses) every ~8us - ~400us.  

    The DLPC7540 controller does not support the ALC features of the DLPC410 that allow specific DMD pattern control, etc..  The DLPC410 does not support or understand live-video or grey-scale data; it only understands binary patterns.

    They are different products for different markets and applications. 

    Regarding moving the mirrors constantly.... The duty cycle of the mirrors has an impact on the lifetime of the product.  There is more information on that in this published paper: Lifetime Estimates and Unique Failure Mechanisms of the Digital Micromirror Device (DMD)  (https://www.ti.com/pdfs/dlpdmd/133_ieeeir.pdf)

    In addition, the DMD datasheets (DLP9500) include recommendations related to duty cycle in a section called "Micromirror Landed-On and Landed-Off Duty Cycle"; they also have a recommendation for derating the operating temperature based on the duty cycle.


    Regards,
    Gary

  • Thanks Gary...I understand the functionality difference  between DLP651NE and DLP9500.... when I ask about DLP9500 differs from DLP651NE... i am asking in regards to DMD micromirrors state ON and OFF. A subject that you and me are talking for couple of days only.... :- )  and you keep telling me on additional materials in regards to functionality... Either case... in regards to DMD micromirrors state ON and OFF, the issue is resolved you did good.... thank you
    Babak

  • Hi Gary
    We followed what you said ... all about PWM and mirrors refreshing whit DLP651NE. He mentioned due to PWM streaming,  mirrors that are stayed in ON/OFF will stay in ON/OFF state 95% and 0.5% will be in OFF/ON state. Gary also helped us and answered my question and mentioned mirrors transition from +/-12 degree to ~4-6 degree and not completely back to OFF/ON  (-/+12) degree. We conducted a test using laser as follows and we noticed mirrors refresh as Gary said. But it refresh fully from 95% in  +/-12 degree (ON/OFF)  back to fully -/+12 degree (OFF/ON) 0.5%  and not ~-/+ 4-6 degree.

    This is causing an issue for us. Can you please advise why mirrors doe full swing 0.5% of the time and not~4-6 degree?

    Is there a way  away to make this 0.5% swing rather than -/+12 degree to -/+4-6 degree?

    here is what we did: 

     Test of laser on DMD==> to proof when we go from ON state to OFF state, what we call "dithering or swing or wiggling of mirrors" does or does not happens and in what percent and how much.

    1- We created a power point presentation with one page all white (to force DMD ON) and one page all black (to force DMD off)

    2- first when DMD is powered off -its micromirrors stays flat and it is called flat state

    3- DMD is turn on while white page was on monitor connected with HDMI to DMD board. then we go on monitor white page-black page-white page -black page... to move mirrors from ON to OFF state.

    As shown in video below, exact same spot that is bright on white page as ON state, will goes dim- NOT OFF- and spot that is dim goes ON bright on black page.

    Note: due to temporal coherent of laser, laser creates may spots but position of spots does not change but dims when power point on monitor goes white (ON)  and black (OFF). since position of a bright spot goes dim it means mirrors are wiggling but in full +/-12 degree and not +/-4-6 degree . If mirrors were wiggling +/-4-6 degree position of dim spot would of changed.   

  • Hi Gary.... we kindly need your input... we are in middle of our project... appreciate for responding above Thanks 

  • Hello Babak,

    mirrors that are stayed in ON/OFF will stay in ON/OFF state 95% and 0.5% will be in OFF/ON state. 

    Just to clarify, these numbers should be approximately ~99.5% and 0.5%.

    > Gary also helped us and answered my question and mentioned mirrors transition from +/-12 degree to ~4-6 degree and not completely back to OFF/ON  (-/+12) degree. We conducted a test using laser as follows and we noticed mirrors refresh as Gary said. But it refresh fully from 95% in  +/-12 degree (ON/OFF)  back to fully -/+12 degree (OFF/ON) 0.5%  and not ~-/+ 4-6 degree.

    > This is causing an issue for us. Can you please advise why mirrors doe full swing 0.5% of the time and not~4-6 degree?

    The movement of ~1/2 way to flat (around 4-6 degrees) is not intentional; it occurs as a side-effect of the video PWM sequence running continuously.  The PWM sequence is always loading and resetting the mirrors every ~8us - ~400us, even if the data is the same.  When the data loaded is the same as the current pixel state, the load and reset (clocking pulse) results in a little "bounce" of around 4-6 degrees (roughly half-way to flat) over roughly 1-2us.. 

    This bounce not intentional; it is a side-effect of how the video applications work with a continuous running PWM sequence.  It has no impact on typical video applications the 7540 is intended for. 

    The 0.5% on/off pulses you are referring to are separate and not related to this bounce... they are intentionally inserted.  As I described in a previous reply:

    There is a pair of mirror transitions inserted once per frame at the start of the first blue segment; they are about 1% of the frame time.  The time is split roughly in half for ON and OFF (i.e. roughly 0.5% ON and 0.5% OFF).  The on time should always be ~0.5%; the off time should be the greater of 0.5% or ~60us for this particular dmd and controller.  You cannot change the duty cycle of these pulses.  

    > Is there a way  away to make this 0.5% swing rather than -/+12 degree to -/+4-6 degree?

    No.  These 0.5% transitions are intentionally inserted and are full on / full off.  We specifically want all of the mirrors to move fully (+/- 12 degrees) at least once per 60Hz frame time, even if the video data is full white or full black for a long period of time.  The illuminators (RGB illuminator enables / strobes) are disabled / off during this time so this is not visible on the screen in a video application.

    Hopefully that clarifies things. 

    Regards,
    Gary

  • Hi Mr. Gary,
    Thanks for response. you did not tell me about once in a 60HZ full tilt/wiggle ...I asked specifically (see through our back and forth communication above), is 0.5% corresponds to +/-12 degree and you mention no it is ~4-6 degree and never mentioned once a 60HZ… ok as long as I know full story I am happy .. thank you.

    Our question is focused merely on tilt and wiggling of mirrors...  so there two types of mirror wiggling/tilt/moves... In a high-level description :
    1- A non-intentional bounce ~1/2 way to flat (around 4-6 degrees) as a side-effect of how the video application and continuous running of PWM sequence.  The PWM sequence is always loading and resetting the mirrors every ~8us - ~400us, even if the data is the same.  When the data loaded is the same as the current pixel state, the load and reset (clocking pulse) results in a little "bounce" of around 4-6 degrees (roughly half-way to flat) over roughly 1-2us.

    2- These 0.5% transitions are intentionally inserted and are full on / full off.  We specifically want all the mirrors to move fully (+/- 12 degrees) at least once per 60Hz frame time, even if the video data is full white or full black for a long period of time.  At the moment of full move (+/-12 degree), the illuminators (RGB illuminator enables / strobes) are disabled / off during this time, so this is not visible on the screen in a video application.

     

    • Please kindly advise if above narrative is correct.
    • Please kindly advise if there is a trigger in controller cart that we can use to know the intentional swing for +/-12 degree. We need to use this to trigger off the light source than shooting it somewhere else.
    • Is the occurrence of once every 60Hz is controllable? can we make it once 30Hz or once 120Hz.
    • Is this occurrence of ever 60Hz going to suddenly change randomly from once 60Hz to 120 Hz or 20Hz… sure there is a little jitter in it maybe every 61Hz as an example…
    • What causing every 60Hz occurrence change to some other rat of change value beyond user command.
    • Is there any other mirror wiggling that I need to know beside of unintentional transition and forced every 60Hz and User acquiring it?

    Thanks for all your support.

    Babak



  • > Thanks for response. you did not tell me about once in a 60HZ full tilt/wiggle ...I asked specifically (see through our back and forth communication above), is 0.5% corresponds to +/-12 degree and you mention no it is ~4-6 degree and never mentioned once a 60HZ… ok as long as I know full story I am happy .. thank you.

    I mentioned that the 0.5% on/off pulses are inserted once per frame in the first blue segment.  I assumed a video frame rate was implied.  60Hz is typical, but it could be 60Hz or 50Hz or 120Hz or something else. 

    > Our question is focused merely on tilt and wiggling of mirrors...  so there two types of mirror wiggling/tilt/moves... In a high-level description :

    > 1- A non-intentional bounce ~1/2 way to flat (around 4-6 degrees) as a side-effect of how the video application and continuous running of PWM sequence.  The PWM sequence is always loading and resetting the mirrors every ~8us - ~400us, even if the data is the same.  When the data loaded is the same as the current pixel state, the load and reset (clocking pulse) results in a little "bounce" of around 4-6 degrees (roughly half-way to flat) over roughly 1-2us.

    Yes.  Keep in mind, this "bounce" assumes the data being loaded was the same as the already-displayed data.  If you are displaying full white or full black, this will happen most of the time.  These are same-side transitions (i.e. we are going from a 1 to a 1 or from a 0 to a 0).  Also keep in mind my previous note that this is a video system with dithering, gamma, color processing, etc..  Even with a full white input, you may see some pixels off sometimes.

    > 2- These 0.5% transitions are intentionally inserted and are full on / full off.  We specifically want all the mirrors to move fully (+/- 12 degrees) at least once per 60Hz frame time, even if the video data is full white or full black for a long period of time.  At the moment of full move (+/-12 degree), the illuminators (RGB illuminator enables / strobes) are disabled / off during this time, so this is not visible on the screen in a video application.

    > Please kindly advise if above narrative is correct.

    Yes... but I would say you haven't mentioned the 3rd case... normal operation... every other possible input that is not full black or full white.  In this case

    • Full ON/OFF transitions - pwm modulation of the mirrors to create the desired grey/color shade per pixel (typically every ~8us to ~400us).  
    • Same-side transitions causing the ~4-6degree "wiggle" when the data loaded to a mirror is the same as its existing state.
    • The inserted 0.5% on and 0.5% off pulses I mentioned causing the entire array to move to on and off (illumination is disabled, so these don't display) once per frame.

    > Please kindly advise if there is a trigger in controller cart that we can use to know the intentional swing for +/-12 degree. We need to use this to trigger off the light source than shooting it somewhere else.

    There are R/G/B LED/Illuminator enables that are used control the illuminators; they are all off when we generate the 0.5% on / 0.5% off pulses.  

    > Is the occurrence of once every 60Hz is controllable? can we make it once 30Hz or once 120Hz.

    As I mentioned, it is generally once per frame for LED/RGB-based illumination (things without a wheel).  60Hz is an example.  However, it is slightly more complicated....  At frame rates less than or equal 47Hz, we frame-rate convert the input to 2x the rate and run a faster PWM sequence, so you would actually see two sets of those pulse per frame at 30Hz.  

    At 120Hz, you would see the 0.5% pulses once per 120Hz frame.

    > Is this occurrence of ever 60Hz going to suddenly change randomly from once 60Hz to 120 Hz or 20Hz… sure there is a little jitter in it maybe every 61Hz as an example…

    As you change frame rates, the embedded software will switch to a different PWM sequence designed for something closer to that rate.   There are various different bins to support different frame rates.  The typical rates of 48Hz, 50Hz, 60Hz, 120Hz, and 240Hz should all run at "1x" and have pwm sequences that run at that rate.  They should all be fine for +/1Hz off the frame rate (i.e. if your 60Hz is really 61Hz, it should work fine). 

    You mentioned 20Hz... 20Hz is not supported.

    > What causing every 60Hz occurrence change to some other rat of change value beyond user command.

    > Is there any other mirror wiggling that I need to know beside of unintentional transition and forced every 60Hz and User acquiring it?

    As I mentioned previously:

    ***This is a video system with gamma, dithering, color processing, etc.; so even with full white, some pixels may be off for short times due to the various algorithms.  

    There are a lot of things going on inside the 7540.  It is a video solution with a lot of different features and processing for video.  If you take a look at the programmer's guide, you may get an video of how much is going on inside.  https://www.ti.com/lit/ug/dlpu082c/dlpu082c.pdf

    I believe I have addressed the initial "dithering and flickering" question as best we can for this product.  At this point, we are well beyond the scope of what is supported for the 7540; it is a video display product for video display applications.  We really cannot document every possible case of the mirrors moving, not moving wiggling, etc..  The 7540 does not offer that level of control of the DMD to the end user.

    If you need that kind of control for your application, the DLP9500 w/ DLPC410 that you already mentioned is likely a better fit for your application; that solution offers that level of control -- that is what it is for.

    Regards,
    Gary

  • Thanks for your response and dearly supporting us beyond.... we are close to reolve this case... few confirmation note need your help on this: 

    1- where is this R/G/B LED/Illuminator enables that are used control the illuminators ... i see something here: See data sheet page 20 DLP65NE https://www.ti.com/lit/gpn/dlp651ne and DLPC7540 https://www.ti.com/lit/gpn/dlpc7540 

    ...please see below is this what you are talking about==> 

    2-  does R/G/B LED/Illuminator enables that are used control the illuminators; will catch up with following rates: "As you change frame rates, the embedded software will switch to a different PWM sequence designed for something closer to that rate.   There are various different bins to support different frame rates.  The typical rates of 48Hz, 50Hz, 60Hz, 120Hz, and 240Hz should all run at "1x" and have pwm sequences that run at that rate. "

    3- Our team 
    showed me the advanced GUI for this eval board for DLP651NE. There are hundreds of settings there, maybe some can reduce the amount of period of flickering (60 Hz 48Hz... 240Hz) or even just fully command to off state (we could test how much this affects our lifetime). They think there are many cryptic settings with little or no documentation, but there is get and set support, so if we can figure out the command we need then it should be something we can set over USB to control board of DLP651NE. could you please advise. (I know I asked you if there is a way to change the PWM set.. or shut down or change flickering.... I told them 10 times I copy past your notes... they keep asking... thanks )

    Thank you

  • >1- where is this R/G/B LED/Illuminator enables that are used control the illuminators 

    The illuminator enables are on the DLPC7540 board.  In the schematic, they are labeled LED_EN_RED/GRN/BLU and are available on J97 or J115:

    DLPC7540EVM Board Design Files (Rev. A)

    >2-  does R/G/B LED/Illuminator enables that are used control the illuminators; will catch up with following rates

    The signals that drive the LED enables are built-in to the PWM sequence; so they will match whatever pwm sequence is running at the time.

    The flash image you have should be for an RGB LED system.  I believe it has ~6 cycles @ 60Hz, and one RGB cycle at 100hz or faster.  So, with a 60Hz input, I suspect you will see 2 cycles in 60Hz; so you should see BGRBGR in one frame.  At 100Hz, 120Hz, 240Hz, you would just see BGR. 

    The color duty cycles are built for a specific LED configuration to get 6500K; so you will not see equal times for red, green, and blue.  I think you will see ~36.1%/45.16%/18.74% R/G/B. Duty cycles (one or more) are selected at design/build time and are built-in to the flash image.  I believe the GUI will let you read the current duty cycle back.

    Note that the the illuminator enables are shifted to account for specific illuminator delays and rise/fall times; so they will not directly with the DMD's on/off time (they will be shifted I believe around 12.2us on the enables and around 3.1us on the disables).

    >3- Our team showed me the advanced GUI for this eval board for DLP651NE. There are hundreds of settings there, maybe some can reduce the amount of period of flickering (60 Hz 48Hz... 240Hz) or even just fully command to off state (we could test how much this affects our lifetime).  They think there are many cryptic settings with little or no documentation, but there is get and set support, so if we can figure out the command we need then it should be something we can set over USB to control board of DLP651NE. could you please advise. (I know I asked you if there is a way to change the PWM set.. or shut down or change flickering.... I told them 10 times I copy past your notes... they keep asking... thanks )

    The advanced gui exposes most of the commands supported in the embedded software.  It is an engineering interface for communicating with that software.  I think everything in it is in the programmers guide (https://www.ti.com/lit/ug/dlpu082c/dlpu082c.pdf). 

    You can turn of some of some of the image algorithms (some of the color processing and gamma).  For what you want, I suspect you should disable all the image algorithms that are available to disable.

    I do not believe it has the ability to disable dithering or the pwm seqencer; those are fundamental to normal (and safe) operation. 

    You should be able to select a full black or full white test pattern (among a few others, I believe).  The PWM sequence should still run and show the behaviors we have discussed above.

    Regards,
    Gary