This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: DLP API Files 64-bit

Part Number: DLP4710EVM-LC

Tool/software:

Dear,

 

I have a question about API Files TI offers.

I downloaded it from this link (https://www.ti.com/tool/DLP4710EVM-LC?keyMatch=&tisearch=search-everything&usecase=hardware)

 

After downloading 'DLP-PICO_DLPC34XX-API' and trying to apply it in my program, I got a problem that CyUSBSerial.lib files seems to work only in windows 32-bit.

 

I want to use it in visual studio 2019 (windows x64, c++), so is there a lib file which is built in windows x64 environment?

Or is there link which I can download this file that works in x64?

 

Thanks :)