Other Parts Discussed in Thread: DLPC410, DLPC910
Tool/software:
Hello,
I am using an FPGA to control the DLPC410 and DLP9500 at high speed.
I want to continue exposing while loading the next image data, but when I ran it at a slow speed to check, I found that the image of the next data loaded was faintly visible in the current image on the DMD.
So, I have some questions :
- Will the loaded data change the mirror angle even if it is not reset?
- If the mirror angle is changing, how long does it take from loading the data until it affects the mirror angle? (50us or more is fine for our purposes.)
- We are planning to develop a product using DLP9500X and DLPC910. Does the same phenomenon occur with DLP9500X?
Current Image before loading next image data. (block 4-9 mirror on, other block mirror off)

Current image after loading next image data.

Next image.

Thanks,
Tanaka