Other Parts Discussed in Thread: DLP7000, , DLPC410, DLPC4430, DLP651LE, DLP5500, DLPC900, DLPLCR55EVM, DLPLCRC900EVM
Tool/software:
Hi, I have a few questions about 13.8um pitch DMDs. Can you confirm if only DLP7000 and DLP550HE have this pitch?
Our application requires larger pitch and height of optical area together with smaller resolution in terms of pixels.
I want to understand to what extend DLP550HE could be useful for binary pattern applications, basically in the area where DLP7000 excels.
What is the realistic binary pattern rate of DLP550HE? If it's capable to do 5kHz it will perfectly fit our application. And finally, our optical power will not exceed 20mW/mm2. Will DLP550HE support this, provided that we make sufficient heatsink ad cooling to keep the DMD in acceptable temperature range.
Thanks!