Other Parts Discussed in Thread: DLPC910, DLPC900, DLP7000, , DLPLCR90EVM, DLPLCRC900DEVM
Tool/software:
Hi,
Customer needs a full working set to test DLP 9000 which could accept the continuous image stream to display image on DLP9000 DMD.
Highest image rate is our preference.
They need a full setup chain including PCB controller (LightCraft), DMD chip and any cables required.
DESCRIPTION :
1.DLP9000 Family of 0.9 WQXGA Type A DMD
2.DLP LightCrafter_ single DLPC910 Evaluation Module
(dual DLPC900 not for continuous streaming?)
They are using DLP7000, would like to test the high resolution.
Please help to advise whether can support.
Thanks
Regards
(ref#QF58F63)