Tool/software:
Hi I am trying to used the DMD as diffraction grating. when I make a grating of 12 pixels on the dmd I see that it diffracts the laser (520) . I see two patterns, one due to blazed grating effect of the dmd ( that is when there is no pattern and light is shine on it, you still see a 2D diffraction pattern). and the other one due to the pattern. However as per theory, the + and - order of the diffracted light should have same power which is not the case. Can someone help me find my mistake?
The mirrors are tilted at 12 degrees, so in order to make the reflected light from dmd to go perpendicular, the laser light falls on it on angle 24 degree. However I put around 30 degrees in my case as it worked for me . Since it is very crucial for me that the power values for both the orders match. Can anyone tell why is it not so?