This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPA3005: Power Solution for DLPA3005

Part Number: DLPA3005

Tool/software:

Dear Members 

The external input power is 24[V]. It cannot be directly applied to the DLPA300A.
I plan to use the DLPA3005 LED at maximum current. Could you recommend a DC/DC converter for 19[V] or 12[V] for the DLPA3005?

[Remark : DLP4701LC + DLP3479 x2 (Master and Slave) + DLPA3005A 

Thanks 

Best Regards