Other Parts Discussed in Thread: DLPC3479, DLPA3005
Tool/software:
Hi,
We use the DLP4710LC/ DLPC3479/ DLPA3005 in out AOI equirement and now we want to TI support the below issue:
1) There are about 3% of DLP products made with DLP4710LC have been found to have noticeable flickering in both the LED and DMD when in Display mode,
whether in Test Pattern or Splash mode. Under normal circumstances, the human eye should see it as almost always on. Is this problem caused by welding issues or defects in the DLP chip?
2) The firmware provided by TI has limited support for custom features. In order to fully utilize the powerful capabilities of DLP, can TI provide custom firmware services