This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC410EVM: DLL Mirror Clocking Pulse

Part Number: DLPLCRC410EVM

Tool/software:

Hello,

I am working with the DLL and trying to get a simple example up and running.

If i understand correctly, in order to display an image on the DMD you first load the data and then apply a mirror clocking pulse to have it display. This can be done in a variety of ways, but for simplicity let's just assume I write all data to the DMD and then want to apply a global mirror clocking pulse. In the ActiveX API there is the Reset Command. However, I can not find in the API the corresponding way to accomplish this with the DLL.

How is a mirror clocking pulse accomplished with the DLL?

Thanks,

- Nathan