This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC231-Q1: Script running misreported

Part Number: DLPC231-Q1


Tool/software:

Script:PD Detection and Analysis_v3_0812.py.

Mainboard:DLPC231+TPS9900

Why there is an error?

  • Hello Hui Xu,

    There is a mismatch in the command arguments. There are two options - You can either use a later version of ACP (v1.60.1.33) where the command is updated.
    Or you can change the script.

    Line 43: Replace with the below line of code
    Summary = WriteTps99000Tia1Trims( 1.0, 1.0, 1.0, False)

    Let me know if you have any issues.

    Thank you,

    With regards,
    Aishwarya