Tool/software:
Currently we have a issue FW download.
There are two kind sample IC of DMD. One is DLP5530HAFYKQ1 and another one is DLP5530SAFYSQ1.
I received DLP composer and project file from TI FAE in KOREA (victor.park@ti.com)
He recommended to install revision 1.12 Release, but that file was blocked to download.
So I downloaded 1.14 Release and installed.
Then I downloaded EVM project marked yellow in below table.
Using that project file, FW building was okay. But according to DMD, booting is normal or abnormal.
In case of using DLP5530HAFYKQ1, booting is okay after FW download to flash memory.
But in case of using DLP5530SAFYSQ1, boot is not complete after FW download to flash memory
Below captures are taken booting fail case.
Could you let me know which points are wrong for DLP5530SAFYSQ1?
I don't have enough q'ty of DLP5530HAFYKQ1 and we have to use DLP5530SAFYSQ1 finally because of support functional safety.
I have to bring up new board as soon as possible. Please let me know some guide to solve this issue.