This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP801XE: DLP801XE

Part Number: DLP801XE
Other Parts Discussed in Thread: DLPC4420, , DLPC4422

Tool/software:

Hi Ti

        I'm Tian from Wintech.We want to use two DLPC4420 to drive the DLP801XE(3840*2400).For the below"Front end IC",which could be used by us?

Thank you very much for any information

Best regards

Tian

       

  • Hello Tian,

    I am assigning this to the person most familiar with the 442x systems.  He is out until Tuesday for the holiday.

    Fizix

  • Hello Tian,

    We leave this for customers to have the freedom to design their system and don't have a recommended Front end IC solution for this chip. This solution also requires a 4K+ (3840x2400) resolution which is comparably niche.

    We recommend customers to reach out to their previously utilized front end IC providers and work with them to find a solution.

    Relatedly, it is possible our recommended 4K UHD solution - IT6807 - front end chip offered by ITE is a solution but to this point has not been tested/verified.

    Best,

    Aaron

  • Hello Aaron,

                      Thank you very much,another question,can we set Front end IC to display 4K+(3840*2400)by DLPC4422' IIC?

    Best,

    tian

  • Hello Tian,

    The DLPC4422 is the predecessor to the DLPC4420 and is a drop-in compatible controller part. 

    The DLP801XE is only included in the latest software updates for the DLPC4420 and the DLPC4422 controller was removed before this DMDs release.

    Additionally, we never provided a front-end solution for the DLPC4422 but it was capable of 4K UHD resolution.

    Again, 4K+ is a niche resolution and it's highly recommended your work with front end IC providers to find a solution - with the DLPC4420 controller.

    Best,

    Aaron