Other Parts Discussed in Thread: DLP2000
Tool/software:
Hello, I'm working on a project where I'm designing a replacement lens for a DLP2000. My goal is to replace the projection lens with a custom-designed relay lens, and I noticed that there is a lens right in front of the DMD that affects both the illumination beam and the beam reflected off of the DMD. My questions are:
- Is the lens right in front of the DMD critical to the illumination? Or can it be removed without significantly affecting the DMD illumination?
- If the lens right in front of the DMD is necessary to keep in place, can the prescription (material, radii of curvature) be shared with me so that I can include it in my custom lens design?
- When designing the custom lens, how do I account for the DMD offset %?
Thank you for your help!