Other Parts Discussed in Thread: DLP4710LC, , DLPA3005
Tool/software:
Hello!
I use a self-made board, the hardware structure is dlp4710lc + dlpc3479 + dlpa3005.
When the Display - External Video Mode is used (05 register is set to 00), RGB888 mode (07 register is set to 43), and the external input is 1280*800@60hz,
Does DLPC4710LC display R[7:0], G[7:0], B[7:0] in sequence? Or some other order?
What is the exposure time for each 8-bit graphic? What is the dark time?
Is the exposure time and dark time the same for each 8-bit graphic?
Please help to analyze the reason, thank you very much!