Other Parts Discussed in Thread: DLP4710LC, , DLPA3005
Tool/software:
Hello!
I'm using External Pattern Mode, 8-bit monochrome patterns。
I'm uses the PARALLEL RGB interface, the timing is RGB888, and the external input is 1920*1080@60hz.
The hardware architecture is dlpc3479 + dlpa3005 + dlp4710lc.
The DLP4710LC can display pictures normally, but TRI_OUT1 has output, while TRI_OUT2 has no output
The following is the register I configured, and the corresponding value, to help me see if there is a problem。
ADDR value
8'h92 8'h02,8'h00,8'h04,8'h00,8'h00
8'h92 8'h03,8'h00,8'h00,8'h00,8'h00
8'h96 8'h02,8'h03,8'h00,8'hA2,8'h14,8'h00,8'h00,8'hE8,8'h00,8'h00,8'h00,8'h29,8'h00,8'h00,8'h00
8'h05 8'h03
Thank you very much!