This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
In description of GPIO Peripheral Interface in DLPC3478 datasheet , GPIO pins must be configured through software for input, output, bidirectional, or open-drain operation. What software is used for configuration? With firmware, how do you do that? GPIO pin control is not seen in I2C interface control. Does the firmware (DLPC3478+DLPA2005) have a default configuration for these GPIOs? What is the default configuration for these
GPIOs?
Hello Paul,
The firmware is responsible for configuring the GPIO pins in accordance with the reference design. Please ensure that you refer to TI schematic as reference for your design. Additionally, please note that the GPIO pins cannot be controlled through the EVM GUI.
Regards,
Kirthi Vignan