Part Number: DLP500YX
Other Parts Discussed in Thread: DLP670S, , DLPC900
Tool/software:
In DLP500YX and DLP670S datasheet
The 8-bit gray pattern rate (prestored patterns with illumination modulation) is 2016Hz and 1190Hz

But in actual testing, the speed is not as high as this.
The testing process is as follows.
1、 Set illumination modulation

2、Load image data and set parameters. For DLP500YX, the minimum exposure time is 1034us, which means the maximum frame rate is 1000000/1024=967Hz. For DLP670S, the minimum exposure time is 944us, which means the maximum frame rate is 1000000/944=1059Hz, much smaller than the values on the document.


I would like to ask what the reason is, is it because we made a mistake in our operation? Or perhaps some other issue.
Thanks
Pan Cheng From Fldiscovery