This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP6500FLQ: DLP6500 active block function question

Part Number: DLP6500FLQ


Tool/software:

Hello TI DLP team,

I'm posting below question from my MM customer on behalf of them(they don't have company email yet). Your kind help would be appreciated.

I have a question about DLP6500.

When I tried to use DMD Active Blocks function, I failed to display patterns on DMD

I tried like this

  1. DMD Active Block setting as below
  2. Select Pattern On-The-Fly mode
  3. Add 3 patterns (1920 x 144 bmp file)

    - I uploaded the pattern, which has 1920x144 resolution first

      and next, I uploaded the 1920x1080 resolution patterns for testing

  1. Click Update LUT buton
  2. Start button click

 

I tried testing 1-bit depth and 8-bit depth pattern each

But I can't see anything on DMD.

Could you let me know what I did wrong?

Regards,

Victor Park