Other Parts Discussed in Thread: DLPC3478, , DLPA3005, DLPA3000
Tool/software:
Hello, Ti team.
We found that in the GUI, reading this temperature was wrong.
The driving board is designed with reference to the EVM board. The temperature reading circuit has confirmed that there is no problem,
but it is 204 degrees every time it is read back.
Moreover, I tried to change the NTC resistor into an adjustable resistor.
The voltage ranged from 0 to 0~1.8V, and it was all 204 degrees after reading. Replacing other driver boards is the same mistake.
The firmware version we used was established by ourselves, including 8.3 and the latest 8.4 version, including 8.0, but it was read incorrectly.
In addition, we also downloaded the version downloaded by TI.COM, which is also a reading error, as shown below.
But in our DLPC3478 driver board, the temperature read back is correct.
So we suspect that there is a bug in the firmware, please solve it, thank you!