This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC230-Q1: DLP5531LEQ1EVM

Part Number: DLPC230-Q1


Tool/software:

Hi, I get the following error starting the DLPC tool:

Crash File for DLPC230 Control Program 1.8 Build 1242 (3142475da8d7)
Current Time: 10/31/2024 1:42:53 PM


Message:


10/31/2024 1:42:53 PM
Exception : Could not load file or assembly 'DLPComposer.SDK.Lite.dll' or one of its dependencies. The specified module could not be found.
Source : InterfaceDefinition
TargetSite : Boolean EncryptToFile(System.String, System.String, Common.ContentType, Common.ArchiveType)
Stack Trace :
at InterfaceDefinition.ApplicationManager.EncryptToFile(String FilePath, String Contents, ContentType ContentType, ArchiveType ArchiveType)
at InterfaceDefinition.ApplicationData.PopulateCurrentMode()
at InterfaceDefinition.ApplicationData.FillApplicationDataSettings()
at ControlProgram.MainForm..ctor(String[] Args)
at ControlProgram.ControlProgramApplication.OnCreateMainForm()
at Microsoft.VisualBasic.ApplicationServices.WindowsFormsApplicationBase.OnRun()
at Microsoft.VisualBasic.ApplicationServices.WindowsFormsApplicationBase.DoApplicationModel()
at Microsoft.VisualBasic.ApplicationServices.WindowsFormsApplicationBase.Run(String[] commandLine)
at ControlProgram.Program.Main(String[] args)
Data :
InnerException : null

It is the same issue as this thread: https://e2e.ti.com/support/dlp-products-group/dlp/f/dlp-products-forum/993239/dlpc230-q1-dlpc230-control-program-wouldn-t-launch

What is the solution? I tried the admin and reinstalling solution in the ticket and it didn't work for me too.

  • Hello Thijs,

    I'm sorry you are running into issues here. I'm getting a professional that can help you with this shortly.

    I appreciate your patience as they respond!

    Best,

    Aaron

  • Hi Thijs,

    I'm very sorry that DLPC230 Control Program does not seem to be working for you.

    May I know what operating system you are using? Do you have the proper Microsoft dependencies installed if you are on a Microsoft Windows OS? As far as I know, this is a Windows-only application, but I could be mistaken.
    Where are you installing this? The default location is "C:\Program Files (x86)\Texas Instruments\DLPC230 Control Program Lite 1.60.1.141"

    I am not as familiar with the software, but my first thought when reading the log is that there is some dependency with Microsoft Visual Basic. This is most likely failing at the start of the main application:

    at ControlProgram.ControlProgramApplication.OnCreateMainForm()
    at Microsoft.VisualBasic.ApplicationServices.WindowsFormsApplicationBase.OnRun()
    at Microsoft.VisualBasic.ApplicationServices.WindowsFormsApplicationBase.DoApplicationModel()
    at Microsoft.VisualBasic.ApplicationServices.WindowsFormsApplicationBase.Run(String[] commandLine)
    at ControlProgram.Program.Main(String[] args)

    Are you able to download the installer once again? Maybe the file was corrupt when you originally downloaded it? I would uninstall one more time, download the installer again from the DLPC230 software development tab, delete the old installer, and then reinstall.

    Then, if this issue persists, check to see if this error appears again. Do you have a coworker or colleague who is able to get a fresh install on their computer to reproduce this issue?

    Aaron,
    Thanks for covering while I was out of office.

    Regards,
    Michael Ly

  • Hi again Thijs,

    A colleague of mine said she has seen this error before. It appears you are missing a dependency (specifically a DLL) after all!

    I will send you a private message if you accept my E2E friendship invitation.

    Regards,
    Michael Ly