This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR95UVEVM: DLPLCR95

Part Number: DLPLCR95UVEVM
Other Parts Discussed in Thread: DLPLCRC410EVM, DLPC900, DLPLCRC900DEVM

Tool/software:

We had previously purchased DLP D4100 0.9" UV 1080P kit.  If it is not sold now, would it be possible to purchase DLPLCRC410EVM and DLPLCR95UVEVM for the same use as DLP D4100 0.9" UV 1080P kit?

  • Hello Takashi-san,

    This is how they are now sold.  You can buy the controller EVM [DLPLCRC410EVM] and the desired DMD EVM [DLLCR95UVEVM - in your case] as needed.

    Therefore the answer to your question is yes this is how you would purchase the equivalent now.

    You will likely need to update the GUI version if you are using the TI GUI.  Also be aware that the GUI has issues with Windows 11.

    Fizix

  • Thank you for your reply.

    I understand that the combination of DLPLCRC410EVM and DLPLCR95UVEVM makes the same configuration as DLP D4100 0.9" UV 1080P kit.
    Let me know two additional points.
    As for the Two 12-inch flex cable, I would like something shorter than 12 inches. Could you tell me what length you have the variety of products?
    Then, TI GUI is about DLP Discovery 4100 Explorer GUI?

  • Hello again Takeshi-san,

    The 6" cables that come with the DLPC900 DEVM kits will also work with the DLPLCRC410EVM,

    Currently we do not sell them separately from the DMD EVMs. 

    Fizix

  • Dear Fizix.

    Thank you for you reply.

    If I want to purchase a combination of DLPLCRC410EVM, DLLCR95UVEVM and The 6" cables, what combination should we order?

  • Takashi-san,

    Regrettably, I do not think we offer them separately or in this combination in the TI store.

    The DMD EVMs come with specific cables.  You might reach out to some of our design partners like Dli, EKB, Wintech, or possible TED (Tokyo Electron Device) in Japan.

    Fizix

  • Perhaps I was mistaken.
    Is it possible to control DLLCR95UVEVM with DLPC900 DEVM? In other words, is there any problem in working DLLCR95UVEVM with DLPC900 DEVM?
    Thank you in advance for your time.

  • Hello again Takashi-san,

    The DLPLCR95UVEVM is not compatible with the DLPLCRC900DEVM.

    Fizix

  • I understand  with that information. Thank you very much.