Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

DLP3010: DLP3010

Part Number: DLP3010

Tool/software:

Hi,

I am planning to use DLP3010 in one of my products which has an operating temperature specification of -20 deg C to +70 deg C.

As the operating temperature for DLP3010 is 0°C to 70° C, I am concerned about the performance of the DLP3010 at negative temperatures.

1. What are the performance deviations which I can expect if DLP3010 operates between 0 degC to -20 deg C for longer duration?

2. Is there any test reports/results which is performed by TI to understand the performance variation & failure rate of the DLP3010 at negative temperature (0 to -20 deg C)?

3. What is the definition of short term operational in the datasheet under section Operating Conditions?

4. May I know the MTBF values calculated for DLP3010?

Best Regards,

Darsana