Other Parts Discussed in Thread: DLP3010, , DLPA2005
Tool/software:
Hello.
I am developing a product by customizing DLPC3478+DLPA2005+DLP3010.
I have two issues to inquire about.
Issue 1.
I am controlling the internal pattern using an external trigger,
but I am curious about the load time that occurs when converting the pattern data shown in the data sheet.
Is the time for number 1 in the figure below constant?
How much time does it take?
In number 2 in the figure, is there no additional delay time other than tdarkPre+DarkPost?

The figure below shows the pattern set configuration currently in use.

Issue 2.
As shown in the figure below, if i configure the pattern in the GUI and click Program and Load Pattern, the existing saved pattern is erased and the pattern is saved in the flash memory, but I am concerned about the life of the flash memory.

If i configure WritePatternOrderTableEntry in the DLP API without using the GUI and control it using WriteInternalPatternControl, will there be no data deletion and writing in the flash memory?