Other Parts Discussed in Thread: DLP4710,
Tool/software:
Hi,
I am trying to use the DLP4710 in a DLP4710EVM-LC with two particular goals:
- I want to have control over a single bit, or, alternatively, over a single pixel of the image, i.e. without using the patterns from the GUI but with custom images
- I would like to see how I can use the EVM with in an arbitrarily long illumination time, i.e. I want the DMD to stay in one position and not move, with continuous monochromatic illumination: no " frames", no dark time, no cycle or repeated pattern whatsoever)
Eventually, I plan on using the DLP4710 with external monochromatic illumination. I now am using the EVM.
I have to admit I have only quickly brushed off the GUI's Python scripting commands and had a quick look at the API - I hope there's an easy way to achieve what I want to do.
Thank you!
Gabriel