This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP670S: I need an EDID file with several different refresh rates.

Part Number: DLP670S
Other Parts Discussed in Thread: DLPC900

Tool/software:

Hello, Ti expert!

I asked the question before, that is, I need to use the refresh rate of 15HZ, which has been used stably in the project.
However, several different refresh rates need to be tested and verified, which are 5HZ, 7.5HZ and 10HZ respectively.

Please provide me the EDID file (DLP670S,HDMI)including the above refresh rate, thank you!

  • Hello Junfa Ye,

    I'm getting someone from my team to respond to this shortly.

    Thank you for your patience!

    Aaron

  • Hello, Aaron,
    Ok, thank you.

  • Hello Junfa,

    We have only validated standard frame rates such as 30 Hz and 60 Hz. Please allow me some more time to check if the DLPC900 can operate at the lower frame rates.

    Thank you,

    Regards,
    Aishwarya

  • Hello Aishwarya

    Yes, thank you. Looking forward to your good news.

  • Hello Junfa,

    Unfortunately, DLPC900 does not lock to the source with refresh rates less than 10Hz. I will mark this thread as resolved since we cannot provide a solution right now.

    Thank you,

    Regards,
    Aishwarya

  • Hello Aishwarya

    OK, thank you.

  • Hello Aishwarya

    Let me ask again, can 10Hz be supported?

  • Hello Junfa,

    Please check with this EDID file. Contains video timings for 10Hz, 15Hz and 30Hz.

    I2C_CONFIG : 0x01 0xA0 0x86 0x01 0x00                  
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x00 0x00 0xFF 0xFF 0xFF 0xFF 0xFF 0xFF 0x00 0x11 0x90 0x00 0xC9 0x00 0x00 0x00 0x00 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x10 0x00 0x22 0x01 0x04 0x83 0x00 0x3E 0x78 0x82 0xEC 0x18 0xA3 0x54 0x46 0x98 0x25 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x20 0x0F 0x48 0x4C 0xFF 0xFF 0x80 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 0x01 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x30 0x01 0x01 0x01 0x01 0x01 0x01 0x3B 0x1B 0x9C 0xA0 0xA0 0x40 0x10 0x60 0x30 0x20 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x40 0x37 0x00 0x9C 0x40 0xA6 0x00 0x00 0x18 0x27 0x12 0x9C 0xA0 0xA0 0x40 0x10 0x60 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x50 0x30 0x20 0x37 0x00 0x9C 0x40 0xA6 0x00 0x00 0x18 0xB3 0x36 0x9C 0xA0 0xA0 0x40 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x60 0x17 0x60 0x30 0x20 0x37 0x00 0x00 0xE0 0x01 0x00 0x00 0x18 0x00 0x00 0x00 0xFC 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x70 0x00 0x44 0x4C 0x50 0x36 0x37 0x30 0x53 0x5F 0x48 0x44 0x4D 0x49 0x0A 0x00 0x4F 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x80 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0x90 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0xA0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0xB0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0xC0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0xD0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0xE0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    DELAY : 0x05 0x00 0x00 0x00                  
    I2C_PASSTHRU : 0x11 0x00 0x01 0xA0 0x00 0xF0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 
    DELAY : 0x05 0x00 0x00 0x00                  
    

    Thank you,

    Regards,
    Aishwarya

  • Hello Aishwarya,
    Ok, I'll test